AXIS#.CANOPEN.PSCALE
Description
Internal position values transferred over fieldbus are converted from native 64-bit values to a maximum 32-bit position value. This parameter sets the resolution/revolution of position values back to the controller.
This value determines the counts per revolution of position values delivered by fieldbus. The default value is 20, which yields 2^20 counts/revolution. This scaling is used for CAN
"Controller area network"
CAN is a broadcast, differential serial bus standard developed for connecting electronic control units. Each node is able to send and receive messages, but not simultaneously PDOs 6063h (Position actual internal value) and 60FCh (Position demand internal value).
Example
With units = counts 32 bit (ie: 2^32 counts/revolution), the default PSCALE of 20, and AXIS#.PL.FB = 2147483648.000 [Counts], which is half of 2^32, meaning a position of 180 degrees. The position actual internal value (6063h) over the fieldbus would be 2^20 / 2 = 524288 counts.
Context
See Scaling.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
1 to 32 |
|
Default Value |
20 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
CANBus and EtherCat
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.CANOPEN.PSCALE | 0x5003h | 0x1 | U8 | 1:1 | - | Read/Write | False |
| AXIS2.CANOPEN.PSCALE | 0x5103h | 0x1 | U8 | 1:1 | - | Read/Write | False |